This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55289: Quiescent current into Vout, clarification needed

Part Number: TPS55289

Hi

I'm designing a battery charger with the TPS55289.

The datasheet provides some information about the quiescent current into Vout:

Quiescent current into VOUT pin
IC enabled, no load, no switching, VIN
= 3.0 V, VOUT = 3 V to 20 V, VFB =
VREF + 0.1 V, RFSW = 100 kΩ, TJ up to
125°C
760-860 μA

  • I take it "IC enabled, no load, no switching" means that the Mode register, OE field is set to "Output disabled"?
  • Does pulling EN Pin low influence the quiescent current into Vout? If so, how large is Iq when the IC is not enabled?

Your help is appreciated.

Tobias