Part Number: BQ27320
Other Parts Discussed in Thread: BQSTUDIO
Hello,
I am using BQ27320 to monitor a Lipo Battery. The system is powering a pulsed load (1.25A pulses, 300ms HIGH, 400ms LOW).
When I monitor the readings from BQStudio I see that the Average Current and Current readings are not accurate. They seem to be getting only the HIGH pulse. This means that the real average current is not correctly represented and the Average Time to Empty is less than it should be.
Is there a way to configure the refresh time for those automatic readings so the BQ27320 can monitor both high and low pulses and make a more accurate estimations?
Thank you very much.