When using an aux supply for VCC, as shown in Figure 9-7 of the datasheet, does the LM5156 disconnect BIAS when the voltage on VCC is higher than VCC-reg?
Thanks,
Stephen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When using an aux supply for VCC, as shown in Figure 9-7 of the datasheet, does the LM5156 disconnect BIAS when the voltage on VCC is higher than VCC-reg?
Thanks,
Stephen
HI Stephen,
thank you for using the E2E forum.
I am not sure what you mean with disconnect. Can you explain in more details?
As you can see in the block diagram there is a diode from VCC to BIAS so if Vcc is higher the BIAS the Diode gets conducting.
Best regards,
Stefan
Hi Stefan,
If you apply an external voltage to the VCC pin such that VCC_reg < VCC < BIAS, will there be any current draw into the BIAS pin of the device?
Regards,
Stephen
Hi Stephen,
no, in this case no current is drawn from BIAS (except some leakage current).
Note: i assume you mean with VCC_reg the regulated output voltage level of the Vcc Regulator as defined in the spec.
Best regards,
Stefan
Hi Stefan,
Thanks, that's what I thought. Do you know if we have an estimate of what that BIAS leakage current would be in this case?
Regards,
Stephen
Hi Stefan,
Gotcha. Follow up question from the customer - is the internal circuitry powered by VCC or does it just power the gate driver? The block diagram doesn't explicitly say whether the amplifiers/comparators are powered by BIAS or VCC.
Thanks,
Stephen
And those would only draw 2-5uA during operation if VCC is supplied externally?
HI Stephen,
main portion of the current would be due to the VCC LDO but if this current is delivered from Vcc, then there is just some small logic left.
E.g. the EN/UVLO logic which is covered by the shutdown current as well.
Best regards,
Stefan