Part Number: BQ24125
Other Parts Discussed in Thread: BQ24171, BQ24133
Hi,
I implemented in my board the power-path selection circuit from the document SLUA376 topology 3. For Q1, Q2 and Q3 I have selected DMP3037LSS-13 and for the third transistor, 2N7002ET1G.
In my board Vin is 9Vcc. The Vbat is the voltage from 2S li-ion cells which during the tests was about 7,8V approximately. The PG/ pin is also connected to a pull-up resistor that was tested tied to 3.3Vcc and also to 12Vcc.
The voltage in Q3 gate changes when I connect the power supply (BATDRV) but Q3 is always ON which causes the voltage from power supply to go directly through the battery with no control of the BQ24125.

What are the suggestions to make this circuit to work correctly ?
Thank you !
Ubiratan





x