Other Parts Discussed in Thread: TPS1HTC30-Q1, TPS272C45
Hi,
My customer is encountering issue where they have two 10W bulbs on the output of the TPS2H160-Q1. With CL = 1.8A, the device goes into constant reset (due to high inrush current). Vs = 24V so steady-state current is around 840mA for the two bulbs. The inrush current of the bulb is about 10x that of steady state, so about 8.4A. When CL = max the current limit does not trip (which is good), but setting CL to max defeats the purpose of the current limit.
My questions are:
-are there any options here to limit in-rush while still using the TPS2H160-Q1?
- or to prevent the current limit from tripping during in-rush period?
I can propose the TPS272C45 but that does come at a higher cost, which also isn't ideal.
Thanks,
Tyler