This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
bq34110 is best for rarely discharged systems.
When used on the system side, it is important to note that putting in new batteries will result in re-initialization.
TRM section 2.7.1 CEDV Gas Gauging Operational Overview states that. "The system must go through a full charge and then a full discharge cycle before the correct FullChargeCapacity() (FCC) is estimated."
This would be used only for a few seconds to gracefully shut the computer down if power is lost to prevent corrupting the image. Allowing the computer to fully charge/discharge if the cells are changed is fine. Would the LEN pin be required to be used or would we be able to allow the computer to drain the cells down to complete the learning cycle?