Hi team,
According to the application note(slave12E),after powering up the tps23881, we need to load sram for tps23881. And then send commends to set the registers from MCU via I2C.But the customers do not want to load sram using the MCU via I2C.
So here are questions from customer,
1. why we need to load the sram after powering up the tsp23881;
2.can I skip such loading?(I find the answer saying it will not pass compliance test and ROM has some slight bugs. );
3.according to the datasheet, the device has auto-mode. In my view, I could load the firmware to the tps23881. And the device would work automatically after re-powering up without loading second time. Am I right?
4.If the customers could not skip the loading sram, can customers add EEPROM with I2C interface where the tps23881 would load sram from EEPROM via I2C? How much is the software used for loading sram?
yours
nan