Hello, please help me figure out what's going wrong with my TPS62737. Thank you.
When I measure the Vout line, it goes up and down from 1.3v to 1.4v.
I checked that it's getting good Vin (4.10v). The EN2 is getting 2.5v from the processor, so it's turned on. And I double checked all the ground connections.
R1: 4.99Mohm
R2: 169Kohm
R3: 7.68Mohm
I used the calculator sheet for resistor values.
VIN is supplied from LiPo battery at 3.7v.
Schematic: