Other Parts Discussed in Thread: DDC316, REF3140, , OPA350, REF35, REF50
Good afternoon,
In one of my designs I am using a DDC316. In the reference schematic in the datasheet of the DDC316 (p.19 Figure 15), an external reference is supplied by a REF3140 and a OPA350. Due to limited space on my design, I would like to use the REF6141 (which has an integrated buffer) instead. However I am struggling a bit with determining if this is a good option regarding noise and stability, since the DDC316 has a 16-bit resolution. Looking at the numbers and calculations, I would say that the REF6141 is the better option to use with the DDC316. Is this correct?
If not; would there be a noticeable difference in performance if I were to use the REF3140 with the DDC316 internal buffer instead of the external OPA350?
Kind regards,
Ramon Jansen