Hi team,
if our one of our 0x20 bit has been triggered,
will it be reset once the issue is gone or it will stay still for a duration of time?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
if our one of our 0x20 bit has been triggered,
will it be reset once the issue is gone or it will stay still for a duration of time?
Hi Fred,
Please see section 9.6.2.1 ChargerStatus Register of the datasheet. Most of the faults are latched until a read from the host. Some of the faults remained latched until the host clears the fault and the state status bits are not latched.
Best Regards,
Jacob
Hi Jacob,
so when a fault is triggered, and then after that we read it even the condition is already cleared in real time , it will still read that latch fault bit but clear the bit to 0 at the same time.
in short, can customer know all the fault history bit that latch when we try to read 0x20?