Hi Team,
ZTE uses TPS7A8401A, and they have some question when using this part.
Test condition: Vin=3.3V, Vout=2.5V, Iout=0.5A; RFB_up=30.1k, RFB_bottom=7.44k, cff=0.01uF
After the LDO normally outputs 2.5V, the load will have a reverse sink current of about 40mA, which will cause the FB voltage to be pulled up to 0.54V, and the output voltage will rise to 2.8V.
Is there any application risk in this way?

Thanks
Brs
Jaydden