Other Parts Discussed in Thread: TIDA-050012, , TPS65981
Hello,
we have developt for a customer an application. In this application, we should load a tablet and at the same time, data should be exchanged from the tablet to a controller. The data exchange should take place via a USB to Ethernet controller. Loading from the tablet via the TPS65987DDHRSHR works.
However, the USB to Ethernet controller is not recognized by the tablet. This is only recognized when we hold the TPS65987DDHRSHR in reset. Data exchange is then possible via the Ethernet controller. As soon as the TPS65987DDHRSHR is no longer in reset, the Ethernet controller is no longer recognized.
Attached is the configuration I created for the TPS65987DDHRSHR
Have you an application note or something similar for such an application?
Alternatively, can you tell me with register is important that power delivery an USB data transfer can work at the same time.smartPLUG04a.pjt