We have custom designed the charger circuit for a RSS smart battery using BQ24765, The functionality on the custom board is working.
But when the board is powered ON, the default charging current is 256mA(approx), we reconfigure charge current to 1 Amps.
Once the DC jack(12VDC) is removed the configured parameters are not retained, the default configuration takes action i.e., 256mA.
The schematics are similar to the BQ24765EVM.
Note: The SMBus PU is to VREF (As per the EVM reference), which is not available after the DC jack is removed.
How do we retain the reconfigured values or how do i change the default value for my custom board.
Thanks
Prasad