Hi Team,
here is a question on auto-switching frequency operation.
During actual test, we find that
a. when the 8-bit MSB < = Low threshold, Fsw changes to 250kHz.
b. when low threshold < the 8-bit MSB <= high threshold, Fsw change to 500kHz
c. when the 8bit MSB > high threshold, Fsw changes to 1MHz.
so it's different with the description as below. Not sure if below is incorrect. Thanks.
BRs
Given