Hi TI team,
I have two issues related to the BQ25792:
- Is there a spec for VSYS output current while on battery? I see IBAT_OCP is 9.3A, so I assume that VSYS can output at least that much current?
- I'm a bit confused on the use of VREGN to set IINDPM. The TIDA-0500047 schematic shows a voltage divider with a note saying it sets IINDPM to 500mA.
- If I use the equation on page 28 of the BQ25792 datasheet and the resistor values on the reference design, I find that VREGN would have to be about 3.3V to set IINDPM to 500mA. This is confusing because VREGN should be regulated to about 4.8V according to the datasheet.
- I am also confused about how VREGN could be used to accurately set IINDPM since it varies so much (between 4.6V and 5.2V depending on the test conditions). Does VREGN have a different value at startup that is more consistent?
Thanks!