This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: BQ34Z100EVM

Part Number: BQ34Z100-R2
Other Parts Discussed in Thread: BQ34Z100

I am using BQ34Z100 EVM, I have configured the gauge for correct cell configuration and was able to calibrate the voltage and current.

The EVM gives correct value of voltage when at rest but as soon as I connect a load the voltage value drops and the shown value does not matches with the multimeter reading.

Similarly as soon as I apply the charging current the voltage value rises and again mismatches with the multimeter reading.

I think this is due to the voltage drop or rise due to internal resistance of the battery, but this should happen at high current values however even when drawing 1 Amp current there is considerable drop in voltage.

How to get accurate voltage? If we don't get accurate voltage how will we be able to protect the cell from overvoltage and undervoltage conditions?

  • Hello Prabhat,

    Check the voltage at the input to the bq34z100 IC and compare it to the voltage reading adjusted with the voltage divider.

  • I have checked in the voltage at the terminal as well it shows the same as the BQ EVM. But my concern is it is not the cell voltage rather it is the terminal voltage.

    What I have observed is that if at no load a  4s battery has a voltage of 14.74V it changes to 15.75 V as soon as a charge current of 1.5 Amps is given, again if the same pack is subjected to a discharge current of 1Amps the terminal voltage drops to 14.44V. 

    How do TI solve this problem of getting accurate cell voltage?

    Because if terminal voltage is only measured then it will trigger false protection of over voltage and under voltage.

  • Hello Prabhat,

    The voltage of the battery will drop under load. Terminal voltage should be set to a value just above where the system will not work. Set the load mode and load select correctly. The algorithm will predict correct SOC based on the load settings. Once battery falls below terminal voltage, SOC will only come up after there is some charge current