This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27546-G1: time to enter hibernate

Part Number: BQ27546-G1
Other Parts Discussed in Thread: BQSTUDIO, EV2400

Hi team,

How long should we expect it to take to for the relaxed cell measurement to put the gauge into Hibernate mode?

Following this process using BQStudio with an eval board:

  • Setting the HIBERNATE bit to 1 and disconnecting the EV2400 from the BQ27546 eval board
    • Hibernate current threshold is set to 8 mA
    • Let the battery cell sit connected to the BQ27546 eval board with no load for > 4 hours and the measured current remained at 65 uA
    • DMM reads 65 uA with a ~ 300 uA draw every 20 seconds

At some point after 4 hours the device goes in to Hibernate mode.

Ben