This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3704-Q1: TPS37042A3OFDDFRQ1 for Monitoring input channel question

Part Number: TPS3704-Q1

Hi, Support Team

We would like to use TPS37042A3OFDDFR-Q1 to replace MAX16133FQP/V+T.

Q1: about TPS37042A3OFDDFR-Q1 could possible use external resistor to change monitoring  to 1.25V/1.25V

Q2: if can chage monitoring voltage to 1.25V/1.25V,  accuracy is 4%?

Q3: TPS37042A3OFDDR-Q1 is best solution?

 

Dual Voltage uP Supervisor

Vendor

MAXIM

TI

Part number

MAX16133FQP/V+T

TPS37044A4OGDDFRQ1

TPS37042A3OFDDFR-Q1

HPC

Main

 

2nd

Part Status

 

 

 

Operation Temperature

-40 to 125

-40 to 125

-40 to 125

Package

SOT23-8

SOT23-8

SOT23-8

EOL schedule

 

 

 

L/T (wks)

 

 

 

MOQ (pcs)

 

 

 

Price

 

 

STLA Used

V

 

 

FXN Used

 

 

 

Note

AEC-Q100

AEC-Q100

AEC-Q100

 

1.71V - 5.5V

1.7V - 6V

1.7V - 6V

reset timeout

10ms

(F)10ms

(F)10ms

Monitoring Input channel

2

4

2

Monitoring Input

1.25v / 1.25V

3.3/1.8/1.15v/1.15v

3.3V/1.25V

Reset

Active-Low, Open-Drain

Active-Low, Open-Drain

Active-Low, Open-Drain

Threshold Accuracy

±1%

±1%

±1%

Dual-Input HYS(%)/TOL Options (%)

0.25 / 11 

0.75%

 

if any suggestion, Please advise me.

Thanks,

Best regards,

Lawrence

  • TPS3704x_ADJ_1p25_Resistors.xlsx

    Hello Lawrence, 

    Based on the requirements I would say the adjustable 2ch variant TPS37042BJOFDDFRQ1 is a better fit for the system. With the use of external resistors monitoring a 1.25V on both channels should not be a problem, I have attached a file which calculates the resistors required to make this possible. Based on the calculation a resistor divider with R2:10k and R1:5.6k should set the correct threshold. Let me know if there is any help required with the resistor tool. 

    Regards, 

    Oscar Ambriz