This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24045: BQ24045 Abnormal charging indication

Part Number: BQ24045


Hi 

The customer design with BQ24045, they use USB to charge 120mAh lithium battery. charging current setting: 120mA, R_ISET = 4.7KΩ, R_PRE-TERM = 2KΩ.

Phenomenon: Charge with a single lithium battery, charge to above 4.2V, and it has been in a trickle state, and the charging indicator CHG red light has been on for more than 24 hours.


Resistor resistance R_ISET = 4.7KΩ, R_PRE-TERM = 2KΩ

Please help check it.

Waiting for your reply.

Thanks

Star

  • Hi Star

    The schematic looks OK.

    BQ2404X family of devices has TTDM mode which will disable termination if TS is open.  R1 (10k) is installed ?

    What is voltage at ISET during this time, indication of current going to battery?