Other Parts Discussed in Thread: TUSB1146, TUSB1146EVM
Hello
Design USB-C Alternate Mode.
Used IC is :
- Power Device TPS65987D
- Linear Re-driver Crosspoint Switch TUSB1146
Electrical diagram is copy of eluviation board TUSB1146EVM.
Before SPI-Flash program I can scan 2pc i2c-addresser.
- TPS65987D 0x20
- TUSB1146 0x44
PD-ic can be debug and configuration with i2c 0x20.
If it take a copy of SPI-Flash eluviation board TUSB1146EVM, then program the SPI-Flash on my design. After programming, full working function on USB-C Alternate Mode.
BUT !
TPS65987D i2c-address cannot be scan and debugging cannot be performed, after SPI-Flash is program with eluviation board SPI-Flash copy.
Note! Eluviation board TUSB1146EVM IC TPS65987D i2c address is not available (TUSB1146 is available).
How I do access TPS65987D i2c address on my design or eluviation board?