Other Parts Discussed in Thread: BQ25713, BQ25713B
Our design requires USB Type-C PD functionality as a Sink and Src (up to 100W). The TPS25750+BQ design works well with our current design with one exception; we also require that our battery be able to be simultaneously charged from a secondary power source (non-USB) while acting as a Sink and providing power to the USB-C port. In our current design we use a BQ part to charge the battery, but we can't share the same BQ part with the TPS25750 since they have conflicting power flow direction requirements. We are looking for suggestions for a topology that would resolve this. The secondary power source has variable power capability, and we currently use the BQ to match the charging current to the available power, so we still need to be able to this.