This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74500-Q1: Design Guidelines - and failure modes

Part Number: LM74500-Q1

We have this design:

100A Input, 12V

Is there anything in the design we should be concerned about?

We are worried about a failure in the charge pump causing higher impedance across the fets (fet body diodes). Is there a way could monitor the driver for failure and fault safely? 

  • Hi Richard,

    The schematics look okay to me except for the FET Vds rating. The TPHR9003NL seems to be 30V rated FET. 

    Is your input a 12V automotive battery ? Also what is the input TVS part number ?

  • It is, what are your thoughts? Bulk capacitance on the output ok? TVS: 5.0SMDJ26CA

  • Hi Richard,

    Circuits connected to12V automotive batter can be subjected to transient voltages as defined by ISO 7637-2 and ISO 16750-2. To withstand these transient pulses, you will have to use either

    1. A 60V rated FET with a single bi-directional TVS like SMBJ33CA. For more understanding , please refer to datasheet section '9.3.1.3 Selection of TVS Diodes for 12-V Battery Protection Applications'  or
    2. A 40V rated FET with two uni-directional TVS connected in back-to-back configuration as shown below. For more understanding on TVS selection while using 40V rated FETs, please refer to section ‘10.2 TVS Selection for 12-V Battery Systems’ of LM74810-Q1 Datasheet.