This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27530EVM: Query on SCl and SDA signal connections

Part Number: BQ27530EVM

Hi,

In our application we are planning to connect BQ27530 SCL and SDA lines to the STM32MP131A MPU. As per BQ27530EVM, SCL and SDA lines are operating at 2.5V but STM32MP131A will support only 3.3V levels. So, can we connect SCL and SDA lines of BQ27530 to 3.3V pull up?

Note: Absolute Maximum Input voltage range for SCL and SDA pins of BQ27530 is 5.5V    

Warm Regards,

Mythili B