hi Teams:
Please help check the schematic diagram of TPS25810, and the requirements are as follows:
1.3A output
2. Can pass USB-C certification
3. The USB-C port only has power when the backend is connected to Device,


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Teams:
Please help check the schematic diagram of TPS25810, and the requirements are as follows:
1.3A output
2. Can pass USB-C certification
3. The USB-C port only has power when the backend is connected to Device,


Kevin,
We will have someone give input by end of the week!
Thanks,
Chris
Hi Kevin,
Thanks,
Field