Other Parts Discussed in Thread: TPS61094
Dear TI experts,
My customer considers TPS61299 for their new product.
I saw the table 7-1 on the datasheet, about Vsel pin configuration.
- 191Kohm for 2.5V output,
- 237Kohm for 2.2V output.
Could you confirm that if I set 200Kohm for Vsel pin?
I am asking it because I thought that I can see the output voltage between 2.5V and 2.2V if I set 200Kohm (probably near 2.5V..)
but my customer said that sometimes they see the output which is very abnormal, even cannot see any voltage.
then what should we do if we need a voltage like 2.4V or 2.3V?
please check this issue. Thanks.
Best regards,
Chase