Other Parts Discussed in Thread: BQ24800
Hi Expert,
Do we have any concern if we use BQ24781R as the 2nd source for BQ24780S?
Could you provide a comparison table for BQ24780S and BQ24781R?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Far,
We recommend to use BQ24800 which is a newer version of BQ24780S. The difference is the BQ24800 has added battery boost mode feature to regulate system power rail above minimum system voltage until battery is fully discharged. There are 4 switching frequency options: 300kHz, 400kHz, 600kHz, and 800kHz. It is pin to pin with BQ24780S.