This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600: How to use

Part Number: UCC25600


For battery chargers, We typically have two feedback loops: one to regulate the maximum charging current and the other to regulate the maximum charging voltage. The loop with lowest error "wins" and controls the output. This gives a CC/CV charging profile.

 Can we use UCC25600 For CC/CV charging by connecting Two feedback loops to DT PIN so that I can set both voltage and current limits?

One more question is my design is Half Bridge LLC resonant converter with the resonant frequency of 153KHZ. In the data sheet given Maximum soft-start frequency is 142KHZ which is very low which might trigger Hugh starting currents at startup. Please clarify...

This IC does not have Input Voltage Sensing. My design has PFC regulated output voltage range ( 385-420V). How the IC will start without detecting input voltage and when will it start? can you give some inputs regarding startup sequence of this IC .

  • Hi Hema Danda,

    Could you use UCC25640x instead of UCC25600. Ucc25640x has much more advanced features compared to UCC25600 like adaptive dead time, charge mode control, ZCS avoidance, burst mode operation, Input UVLO protection etc.

    We do have a reference design for battery charger application using this particular controller.

    PMP40766 Schematic

    Let me know if you have any further questions.

    Regards

    Manikanta P