I am currently experimenting with the TPS25980x. I made a finger-fumble on a scope while probing that pin and I may have shorted to either side; forgot to add test points on that pin. End result is that the eFuse is no longer starting up.
Does anyone know if a GND or VIN (in our case, VIN is 12VDC) signal on dVdT would damage the part? The datasheet is not helpful on absolute limits of that pin.
(TI support pointed me to the function of the pin. Please note that I am interested in max/min voltage, not capacitance).