This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25172: Charge operation temperature range for each NTC

Part Number: BQ25172


Dear in-charge person

In this device specification sheet, recommended NTC is 103AT-2 when charging operation at 0°C to 45°C.

103AT-2 spec are following 

      Resistor @ 25℃ is10kΩ

      B value is 3434K

We can only arrange the following NTC.
Please let me know charge temperature range when using the following NTC.

NCP15XH103D03RC(MURATA)  10kΩ / B value 3380k

https://www.murata.com/ja-jp/products/productdetail?partno=NCP15XH103D03RC

NCP15XV103J03RC(MURATA)   10kΩ / Bvakue 3900k

https://www.murata.com/ja-jp/products/productdetail?partno=NCP15XV103J03RC

Best Regards.