Dear in-charge person
In this device specification sheet, recommended NTC is 103AT-2 when charging operation at 0°C to 45°C.
103AT-2 spec are following
Resistor @ 25℃ is10kΩ
B value is 3434K
We can only arrange the following NTC.
Please let me know charge temperature range when using the following NTC.
NCP15XH103D03RC(MURATA) 10kΩ / B value 3380k
https://www.murata.com/ja-jp/products/productdetail?partno=NCP15XH103D03RC
NCP15XV103J03RC(MURATA) 10kΩ / Bvakue 3900k
https://www.murata.com/ja-jp/products/productdetail?partno=NCP15XV103J03RC
Best Regards.