Hello,
Referencing slva257a and slvu243
If I configure a TPS5430 for negative output (between -3.3V and -15V), does that change the Vin range for the TPS5430.
Typically Vin is 5.5 to 36V (referenced to GND)
Does that change as GND is now the -Vout?
so if I have a -3.3Vout, can I run that from a Vin of 5V?
Thanks for your insight.
-Kevin