Other Parts Discussed in Thread: TPS543A26
1) For IC TPS542A52 the recommended layout given in the datasheet is as shown below, here the AGND and PGND is been connected using a plain, Is it okay to use one OE resistor instead of the plain and connect the PGND and AGND on the other side of the IC as shown in the layout reference.
2) Same for the TPS54824RNV in the recommendation the PGND and AGND are been connected through a single point far from the Inductor, Is it okay to use an OE resistor to connect the PGND and AGND as shown in the layout reference.