Hi team,
Please help to answer the following questions about the TPS4H000-Q1 chip: 1. What is the output capacity of each channel independently? 2. We set 4 channels to output a current of about 500mA at the same time, and the total output current of the chip will be clamped at about 1.3A;
3. The two channels are set to output 700mA at the same time, the chip is clamped to 500mA output, and the output will enter the thermal protection mode after a period of time;
The output current is always limited to unexpected current. Could you help solve this issue?