Other Parts Discussed in Thread: LM51551
Hi Team,
My customers are using LM51551-Q1 to generate a 18V voltage from a 12V battery. However, during start up when the Vin is only 6V the LM51551 cannot successfully start up and the output waveform is like triangle wave.
However when 12Vin start up and then turn the Vin down to 6V the device works normal. The input current during 6Vin start up is about 2.4W and the schematic is as below.

Pls help to check out what may cause this kind of start up problem and how can we fix it, thanks!
BR,
Manu