This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4H000-Q1: Clarifications required Current sensing

Part Number: TPS4H000-Q1

Dear Team,

The output current of this IC is 750mA.

In the detailed design procedure we can see the below things.

May I know what you mean by nominal current(250) here. Does it mean if load current is more than 250mA the device shows fault condition.

"To set the adjustable current limit value at 2.5-A," Does it mean if load current is more than 250mA the device shows fault condition.

My load can take maximum of 650mA .Can i use the values of Rcs and Rcl as given in the datasheet.

Regards

HARI