This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25148: Over current protection range

Part Number: LM25148

Hi,

We use the over current protection function of the LM25148 controller. But it doesn't work well, like the current trip range is pretty wide.

For example, the output voltage drops at 3.5A and the system totally shuts down at 4.3A. The chopping frequency is set at 500KHz. 

Any ideas will be helpful.

Thanks,