Other Parts Discussed in Thread: UCC21750, OPA333
Dears:
Customer want to connect a Amplifier to UCC21750's AIN Pin, As their is 200uA constant current source in AIN Pin, please help check if this way can work well. Thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears:
Customer want to connect a Amplifier to UCC21750's AIN Pin, As their is 200uA constant current source in AIN Pin, please help check if this way can work well. Thanks.

Hi Haiwen,
Yes an amplifier is a great idea if your sensor has a high-Z output. It looks like you have a difference amplifier configuration, and Vref (top of R677) is ground. Is the input signal differential? The input range of AIN is 0.6V to 4.5V, so maybe you should use a 2.5V Vref instead. For this purpose, you could use a 20k +20k resistor divider from 5V to 0V to create a 10k, 2.5k Thevinin equivalent Vref.
OPA333 would be a good high precision amplifier for this task.
Best regards,
Sean