This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am sorry to ask so many questions, but I would like to double check something regarding the zero volt charging of the BQ29700.
My battery protection circuit looks like this
The rest of the power section looks like this
My battery manufacturer has UN38.3 and UL certified batteries, but only with the built in protection circuits. These batteries are delivered in a "shipping mode" that clamps the voltage to around 0.5v until a charger is connected.
Lookign at the datasheet for the BQ29700 it appears the zero voltage charging is actually disabled below 0.75v. Which I think might be a problem.
If I connect USB power to charge the battery through the BQ27074 and BQ29700, with the battery in its shipping mode, will the BQ24074 + BQ29700 be able to bring it out of shipping mode?
Thanks again for your help
-Jason
Hi Jason,
Unfortunately, the BQ2970 will not allow the battery to charge if the battery voltage is < 0.75V. This will place the device in the inhibit region, which prevents 0V charging. If the BQ2970 senses a battery voltage below 0.75V, then the COUT pin will be pulled LOW, and the CHG FET will not be able to turn ON.
Best,
Andria
Ok. That's very disappointing but thank you!
Are there any TI alternatives I could consider?
Hi Jason,
Unfortunately, we do not have a protector or monitor that can do charging on a cell starting with such a low voltage. I can assign this thread to the gauges team, though. They may be able to help if you are interested.
Best,
Andria
That's ok. Perhaps there is another way to do this.
Thanks for your help, you have saved me 6 weeks and ~$500 in prototype costs!
Kind regards,
-Jason