Other Parts Discussed in Thread: TPS53676
Dear Team,
1. When the pin11 and pin12 input current monitoring function is used, is this connection correct? At present, we use four 1moh sampling resistors in parallel for sampling. Do we need to match this parameter in CODE? Where does it match? Is there any reference design specification for this application and send it to us for reference?
2. At present, we use AKIP and BSKIP to connect to the EN pin of DRMOS to enable DRMOS on the board. What is the function of this connection? In the past, the EN of DRMOS was directly connected to the VDD pin of DRMOS, which connection method would you recommend?
3. Does TPS53679 support AVS voltage regulation? The LOOPA load chip in our schematic diagram needs AVS voltage regulation. Please help to confirm whether this design in our schematic can realize voltage regulation. Thank you!
Many Thanks,
Jimmy