This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63901: Vout adjustment (fine trimming) with R2D resistors

Part Number: TPS63901

Hi,

As recommended by datasheet - I am using RCFG1/2/3 resistors with a tolerance of ±1%, temp coefficient better than ±200 ppm.

However, for my nominal selections of (SEL=High) 1.8V (CFG1=0-ohm), I get 1.794V, - and - for 3V (CFG3=13.3K), I get 2.997V.

So, my question is - in order to avoid potential risk of triggering brown-out on certain parts powered by this buck-boost; can I use 
resistor values slightly (few ohms) higher than the nominal values listed in Table 7-2 and 7-3? Such as 10-100 mOhm in place of 
0-ohm.

Please advise. Thanks for your timely attention and help.