This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
can you please share an internal register map and descriptions for the TPS25762-Q1? We want to access these registers over I2C2 from a system MCU and get the diagnostic data, similar to EVM. Is there some programming manual I'm missing? The GUI programming is fine for basic functionality evaluation, but kinda useless for any more complex system design.
Thank you.
JD
Hi JD,
We have not published a reference manual at this time. For diagnostic information such as that found in the GUI telemetry tab, I have included register information below. Be advised reading or writing any other register is prohibited and may compromise device performance.
Bits | Name | Description |
Bytes 6-12: Telemetry | ||
55:48 | VntcVoltage | VNTC voltage ADC reading (0.014 V LSB) |
47:40 | VbusCurrent | VBUS current ADC reading (23 mA LSB) |
39:32 | VbusVoltage | VBUS voltage ADC reading (0.098 V LSB) |
31:24 | VinVoltage | VIN voltage ADC reading (0.08 V LSB) |
23:16 | IntDCDCCurrCode | Internal DCDC Current code reading (25 mA LSB) |
15:0 | IntDCDCVCode | Internal DCDC Voltage code reading (10 mV LSB) |
Bytes 1-5: Reserved | ||
39:0 | Reserved | Reserved. Read value from this location not valid. |
The preceding content is intended as information only and not a part of the device specification.
Refer to datasheet figure 9-38 for I2C formatting.
Hi Erik,
thank you. This should be sufficient. I'm sure you have your reasons, but please reconsider publishing reference manuals.
Regards,
JD