Other Parts Discussed in Thread: UC3845, UC3843
We are building an MPPT tracker using the UC384* Family.
The tracker takes a voltage from 100V to 300V and outputs constant current with a voltage limit of 350V. The current is regulated at the primary side (10A peak), so naturally the output will vary based on the available current and voltage.
The circuit seems to work well, but I want to increase the switching frequency to some 50Khz. Whenever I go past around 10Khz, I start to have a pulse starting and stopping shortly after or some sort of jitter that increases the Mosfet temperature. I tried to clamp the sense voltage feedback, thinking it could be noise, but the problem persists.

Here we can see the gate signal (blue) and the oscillator ramp (yellow).

Here we see the gate signal and the inductor current.
I believe that this is some problem with the compensation. Swapping to a UC3845 resolves the strange pulse behaviour, but naturally I am limited to 50% duty. It also only seems to do full width pulses, skipping when necessary, instead of reducing the duty cycle.

I'm using the following compensation scheme with C = 100pF and R = 150K
I have also tried to use the power stage designer tool, but seems more suited to offline converters? Or perhaps I'm not fully sure what to look out for!