This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25611D: Can't charge with wall charger, STAT led blinks very fast

Part Number: BQ25611D


Hello,


I have a strange issue with BQ25611D. The charger is only working using a PC or a lab power supply (without D+/D-) to charge. Otherwise (using a regular wall charger), the STAT LED is blinking very fast (way faster than 1Hz) and the charge current is not stable at all. Here is a video:

Video

The STAT LED is the white one. As you can see on the USB tester, the D+/D- values are pretty weird too, I don't know if it's related ?

I tried 3 different wall chargers with differents cables: same issue. I checked if the issue occurs on all charging states: it seems to only happen in fast charge mode. I tried to reset to default settings: same issue. I tried on two different boards: same issue. I tried to force the input current setting every second and I managed to get one of my wall charger to work 80% of the time, but no luck for the others and that's not the behavior I'm expecting, I was hopping to let the source detection do the job. I watched for status registers and measured the current while charging, here are the results:

Laptop USB (working properly):

  • Charging state: 2 (fast charge)
  • VBus good: 1
  • VINDPM_STAT: 0
  • IINDPM_STAT: 1
  • BATSNS_STAT: 0
  • Input current: 482mA
  • Input voltage: 5.01V
  • Current going to the battery: 487mA (there is a ~300mA load already plugged, but the issue is the same without load)
  • Battery voltage: 3.09V (LiFePo4)

Wall charger (doesn't work) :

  • Charging state: 0
  • VBus good: 1 (??)
  • VINDPM_STAT: 0
  • IINDPM_STAT: 0
  • BATSNS_STAT: 0
  • Input current: moves a lot between 150mA and 450mA sometimes
  • Input voltage: 5.11V
  • Current going to the battery: -0.03mA (there is still the same load, and the battery is slightly discharging instead of charging)
  • Battery voltage: 3.07V (LiFePo4)

Here are the settings that I use, but as I said, even with default settings I have the same issue.

const uint8_t CHARGING_INPUT_CURRENT{0b00000111}; // Charging current, see 9.5.1 in https://www.ti.com/lit/ds/symlink/bq25611d.pdf // 700mA default input current (updated with source detection)
const uint8_t CHARGING_VOLTAGE{0b00001010}; // Charging voltage setting, see 9.5.5 in https://www.ti.com/lit/ds/symlink/bq25611d.pdf // 3.590V with 15 minutes top off timer
const uint8_t CHARGING_FAST_CURRENT{0b00100001}; // Fast charge current, see 9.5.3 in https://www.ti.com/lit/ds/symlink/bq25611d.pdf // 1980mA fast charge, 500mA boost (OTG/charging?)
const uint8_t CHARGING_PRE_TERMINATION_CURRENT{0b01000010}; // Pre-charge and temrination current, see 9.5.4 in https://www.ti.com/lit/ds/symlink/bq25611d.pdf // 240mA pre-charge, 120mA termination
const uint8_t CHARGING_CONTROL_1{0b10001101}; // Charger control, see 9.5.6 in https://www.ti.com/lit/ds/symlink/bq25611d.pdf // JEITA Vset to Vreg, watchdog disabled, 90°C thermal regulation
const uint8_t CHARGING_CONTROL_2{0b11100000}; // Charger control, see 9.5.7 in https://www.ti.com/lit/ds/symlink/bq25611d.pdf  // VINDPM to 3.9V (minimal input voltage?)

Here is my schematic:

(+3V0 is my LiFePo4 battery)


Do you have any idea of what should I do to fix this?

Best regards,

Gauthier

  • Hello, Gauthier

    Table 9-5 in the datasheet, indicates that it could be input over-voltage, TS fault, safety timer fault or system over voltage.

    if this was already checked would it be possible to send a screenshot of the register values?

    V/R

    Rafael Camarillo

  • Hello Rafael,
    Thank you for your reply. Sadly, this is the first thing I checked before posting. Also, as you may see in the video, the LED doesn't blink at 1Hz at all, it's a random patern that is way faster. I will send you a screenshot tomorow if you prefer to be sure.
    Best regards,
    Gauthier

  • Hi Gauthier, 

    Thank you for providing detailed information regarding the behavior you are observing. 

    I believe the STAT led blinking you are observing is the device transitioning back and forth between charging and not charging status. This is likely due to the issues you are observing with D+/D- detection.

    The device repeatedly starting and stopping charge explains the non stable input current and why the STAT blinking is in a random pattern. 

    Do you happen to have a BQ25611DEVM available where you can test plugging in the different wall adapters and see if the same behavior is observed? 

    Additionally what is the expected detection from the wall adapters?

    I don't think this is necessarily related to the behavior you are observing, but reviewing your schematic the VBUS pin requires at least a 1 uF capacitor. Also does your battery have a NTC which is also connected from TS to GND? Otherwise your schematic looks good. 

    Best Regards,

    Garrett 

  • Hi Garrett,
    Thank you for your reply. Yes I also think it's related to D+/D- detection. I do not have a dev module, but I will buy one to be sure that's the issue is related to my design. I'm using 4 diffenrent wall adapters : a Samsung phone charger, a Xiaomi phone charger, a Raspberry Pi PSU and a no name usb charger. None of them can be used with the charging IC.
    Indeed I missed the 1uF capacitor, I've added it to my design. Yes on the battery side there is a NTC that seems to work properly (while charging, NTC fault is in "warm" state). Thank you for the schematic review.
    I will post a reply to this thread when I'll have more infos about my issue.
    Best regards,
    Gauthier

  • Hi Gauthier, 

    Thank you for the update. I will look out for your reply. 

    Best Regards,

    Garrett