This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: Question about package qty/Carrier of TL431AILPR

Part Number: TL431

Hello guys,

One of my customers ordered TL431AILPR.

At this moment, they have the following question about package qty/Carrier of the ordering number device as the follows.
Could you please give me your reply?

Q1, What is TL431AILPR carrier? Is it tape & reel, ammo or bulk?

Q2. If Q1 answer is tape & reel, will formed lead type be delivered to the customer because TL431 datasheet version SLVS543Q says that "a. Straight lead option available in bulk pack only. "
       and "b. Formed lead option available in tape and reel or ammo pack." on page 82?

Q3. When the customer wants order TL431 straight lead type with tape/reel carrier, what ordering number do they need to use?
       Also when the customer wants order TL431 formed lead type with tape/reel carrier, what ordering number do they need to use?

Your reply would be much appreciated.

Best regards,
Kazuya.

  • Hello Kazuya,

    The TL431AILPR is in a 2000 qty tape and reel. Yes it should be formed lead.

    Unfortunately there is no option for a straight lead tape and reel.

    If the customer needs a straight lead TO-92, they will need to order the TL431AILP in the bulk package.

    Best,

    Walter