Please help to recommend suitable applycation IC
Design concept
VIN is Type C Connector when plus in pass though efuse into USB_VBUS pin comuiate with CPU.
Then CPU Will notify Type C Which Voltage 5,9,12V need to be supplies as input.
1. The Efuse need wide range Vin , if could auto set OCP when difference input is better.
2. The DC-DC(Buck) need wide range Vin could cover minmux on time & hight SW Rating ,ROVP (reverse voltage protection).
3. The BOOST need low IQ, the vin will 1V~3V