Hello Sir/Mam
Can we use Part TPS53667RTAT with four CSD95410RRBT? for Iout=136A and Vout=0.88V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sir/Mam
Can we use Part TPS53667RTAT with four CSD95410RRBT? for Iout=136A and Vout=0.88V
Hello,
Yes that's a reasonable combination. The CSD95410 power stage is rated to 40A RMS, so four of them would have a combined max RMS of 160A.
Thanks,
Travis
Hello,
Can we use Part TPS53667RTAT with four CSD95410RRBT? for Iout=165A and Vout=0.88V.
Hello,
Is the 165A peak current or RMS? If it is 165A peak current & the RMS is lower, that is fine. If it is 165A RMS, that slightly exceeds datasheet specs.
Thanks,
Travis