Hi
The customer test with BQ27Z746EVM-047, When CTOS protection is not triggered, as long as FET is enabled, XCHG and XDSG will be triggered, and can not charge and discharge.
Please help check the attached screen and log file.
Wed Aug 30 17:01:24 CST 2023
Device Version Info = 1746_0_01
BQZ Device Name = bq27z746
BQZ Firmware Version = 0_01
Sample,DateTime,ElapsedTime,ManufAccess,@Rate(@),@TimeEmpty,Temperature,Voltage,Current,AvgCurr,AvgPow,RSOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeFull,MaxLoadCurrent,MaxLoadTimeEmty,VoltHiSet,VoltHiClear,VoltLoSet,VoltLoClear,TempHiSet,TempHiClear,TempLoSet,TempLoClear,SOCDeltaSet,BTPDsgSet,BTPChgSet,IntStatus,ChgCurr,ChgVolt,QmaxCC,TermV,BattStat,CycleCnt,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,BattSenseOutput,BattSenseStatus,SafetyAlert 1,SafetyAlert 2,SafetyStat 1,SafetyStat 2,Elapsed Time,PackPinV,CellVolt,CellCurr,CellPower,IntTemp,TS1Temp,TS1Temp,CellTemp,FETTemp,Cell1RawV,CellRawI,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,CompRes1,PackGrid,LStatus,CellGrid1,StateTime,DOD0_1,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,QMax1,QMaxDOD0_1,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus
1,2023-08-30 17:01:28,4.003,0x0054,0,65535,26.4,3891,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6631,3887,3891,0,0,26.0,26.4,-273.2,26.4,-273.2,3891,3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2234,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1013,SUCCESS
2,2023-08-30 17:01:32,8.010,0x0054,0,65535,26.4,3891,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0440,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6635,3887,3890,0,0,26.2,26.3,-273.2,26.3,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2238,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1068,SUCCESS
3,2023-08-30 17:01:36,12.025,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6639,3887,3890,0,0,26.2,26.3,-273.2,26.3,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2242,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1022,SUCCESS
4,2023-08-30 17:01:40,16.034,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6643,3887,3890,0,0,26.1,26.3,-273.2,26.3,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2246,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1028,SUCCESS
5,2023-08-30 17:01:44,20.048,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6647,3888,3890,0,0,26.0,26.3,-273.2,26.3,-273.2,3890,-6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2250,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1030,SUCCESS
6,2023-08-30 17:01:48,24.052,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6651,3888,3890,0,0,26.0,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2254,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1041,SUCCESS
7,2023-08-30 17:01:52,28.067,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0440,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6655,3887,3890,0,0,26.0,26.3,-273.2,26.3,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2258,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1026,SUCCESS
8,2023-08-30 17:01:56,32.077,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6659,3887,3890,0,0,26.0,26.3,-273.2,26.3,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2262,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1048,SUCCESS
9,2023-08-30 17:02:00,36.081,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6663,3888,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2266,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1030,SUCCESS
10,2023-08-30 17:02:05,40.093,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6667,3888,3890,0,0,26.0,26.4,-273.2,26.4,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2270,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,999,SUCCESS
11,2023-08-30 17:02:09,44.102,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6671,3886,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,-6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2274,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1071,SUCCESS
12,2023-08-30 17:02:13,48.116,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0440,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6675,3887,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2278,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1055,SUCCESS
13,2023-08-30 17:02:17,52.124,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6679,3887,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2282,5103,-28,-11,10,0,2614,5103,-28,10,2.0,1000,4832,2426,882,1018,SUCCESS
14,2023-08-30 17:02:21,56.132,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6683,3888,3890,0,0,26.2,26.4,-273.2,26.4,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2286,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1026,SUCCESS
15,2023-08-30 17:02:25,60.133,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x04,0x0000,0x0000,0x0000,0x0000,6687,3886,3890,0,0,26.2,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2290,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1040,SUCCESS
16,2023-08-30 17:02:29,64.146,0x0054,0,65535,26.5,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x04,0x0000,0x0000,0x0000,0x0000,6691,678,3890,0,0,26.1,26.5,-273.2,26.5,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.5,1000,0,0,5,0,2294,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1014,SUCCESS
17,2023-08-30 17:02:33,68.153,0x0054,0,65535,26.5,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0440,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6695,26,3890,0,0,26.1,26.5,-273.2,26.5,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.5,1000,0,0,5,0,2298,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1007,SUCCESS
18,2023-08-30 17:02:37,72.165,0x0054,0,65535,26.5,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6699,26,3890,0,0,26.1,26.5,-273.2,26.5,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.5,1000,0,0,5,0,2302,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1037,SUCCESS
19,2023-08-30 17:02:41,76.173,0x0054,0,65535,26.5,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6703,1,3890,0,0,26.1,26.5,-273.2,26.5,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.5,1000,0,0,5,0,2306,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,998,SUCCESS
20,2023-08-30 17:02:45,80.174,0x0054,0,65535,26.5,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6707,0,3890,0,0,26.1,26.5,-273.2,26.5,-273.2,3890,-6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.5,1000,0,0,5,0,2310,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1012,SUCCESS
21,2023-08-30 17:02:49,84.181,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6711,0,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2314,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1038,SUCCESS
22,2023-08-30 17:02:53,88.193,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0440,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6715,0,3890,0,0,26.0,26.4,-273.2,26.4,-273.2,3890,-6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2318,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1025,SUCCESS
23,2023-08-30 17:02:57,92.193,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6719,0,3890,0,0,26.0,26.4,-273.2,26.4,-273.2,3890,-6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2322,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1026,SUCCESS
24,2023-08-30 17:03:01,96.197,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6723,0,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2326,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1066,SUCCESS
25,2023-08-30 17:03:05,100.212,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6727,0,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2330,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1007,SUCCESS
26,2023-08-30 17:03:09,104.221,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6731,0,3890,0,0,26.0,26.4,-273.2,26.4,-273.2,3890,-6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2334,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,982,SUCCESS
27,2023-08-30 17:03:13,108.227,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0440,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6735,0,3890,0,0,26.2,26.5,-273.2,26.5,-273.2,3890,6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2338,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1056,SUCCESS
28,2023-08-30 17:03:17,112.236,0x0054,0,65535,26.5,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6739,0,3890,0,0,26.2,26.5,-273.2,26.5,-273.2,3890,6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.5,1000,0,0,5,0,2342,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1016,SUCCESS
29,2023-08-30 17:03:21,116.239,0x0054,0,65535,26.6,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6743,2825,3890,0,0,26.1,26.6,-273.2,26.6,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.6,1000,0,0,5,0,2346,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1011,SUCCESS
30,2023-08-30 17:03:25,120.245,0x0054,0,65535,26.6,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6747,3812,3890,0,0,26.1,26.6,-273.2,26.6,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.6,1000,0,0,5,0,2350,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1052,SUCCESS
31,2023-08-30 17:03:29,124.252,0x0054,0,65535,26.7,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6751,665,3890,0,0,26.2,26.7,-273.2,26.7,-273.2,3890,-6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.7,1000,0,0,5,0,2354,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1047,SUCCESS
32,2023-08-30 17:03:33,128.260,0x0054,0,65535,26.7,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0440,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6755,26,3890,0,0,26.2,26.7,-273.2,26.7,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.7,1000,0,0,5,0,2358,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1053,SUCCESS
Wed Aug 30 17:04:29 CST 2023
Device Version Info = 1746_0_01
BQZ Device Name = bq27z746
BQZ Firmware Version = 0_01
Sample,DateTime,ElapsedTime,ManufAccess,@Rate(@),@TimeEmpty,Temperature,Voltage,Current,AvgCurr,AvgPow,RSOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeFull,MaxLoadCurrent,MaxLoadTimeEmty,VoltHiSet,VoltHiClear,VoltLoSet,VoltLoClear,TempHiSet,TempHiClear,TempLoSet,TempLoClear,SOCDeltaSet,BTPDsgSet,BTPChgSet,IntStatus,ChgCurr,ChgVolt,QmaxCC,TermV,BattStat,CycleCnt,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,BattSenseOutput,BattSenseStatus,SafetyAlert 1,SafetyAlert 2,SafetyStat 1,SafetyStat 2,Elapsed Time,PackPinV,CellVolt,CellCurr,CellPower,IntTemp,TS1Temp,TS1Temp,CellTemp,FETTemp,Cell1RawV,CellRawI,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,CompRes1,PackGrid,LStatus,CellGrid1,StateTime,DOD0_1,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,QMax1,QMaxDOD0_1,QMaxPassedQ,QMaxTime,Tk,Ta,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus
1,2023-08-30 17:04:33,4.005,0x0054,0,65535,26.2,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0440,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6815,3888,3890,0,0,26.1,26.2,-273.2,26.2,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.2,1000,0,0,5,0,2418,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1061,SUCCESS
2,2023-08-30 17:04:37,8.012,0x0054,0,65535,26.2,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6819,3888,3890,0,0,26.1,26.2,-273.2,26.2,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.2,1000,0,0,5,0,2423,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1113,SUCCESS
3,2023-08-30 17:04:41,12.014,0x0054,0,65535,26.2,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6823,3888,3890,0,0,26.1,26.2,-273.2,26.2,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.2,1000,0,0,5,0,2426,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1020,SUCCESS
4,2023-08-30 17:04:45,16.027,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6827,3887,3890,0,0,26.2,26.3,-273.2,26.3,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2430,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1010,SUCCESS
5,2023-08-30 17:04:49,20.028,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6831,3887,3890,0,0,26.2,26.3,-273.2,26.3,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2434,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1040,SUCCESS
6,2023-08-30 17:04:53,24.031,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0440,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6835,3887,3890,0,0,26.2,26.3,-273.2,26.3,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2438,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1038,SUCCESS
7,2023-08-30 17:04:57,28.033,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6839,3887,3890,0,0,26.2,26.3,-273.2,26.3,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2442,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1003,SUCCESS
8,2023-08-30 17:05:01,32.047,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6843,3888,3890,0,0,26.1,26.3,-273.2,26.3,-273.2,3890,-9,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2446,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1031,SUCCESS
9,2023-08-30 17:05:05,36.062,0x0054,0,65535,26.3,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6847,3887,3890,0,0,26.2,26.3,-273.2,26.3,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.3,1000,0,0,5,0,2450,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1021,SUCCESS
10,2023-08-30 17:05:09,40.071,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,4004,4400,0,2500,0x00C0,0,97,0x8186,0x0040,0x10,0x0004,0x40,0x2819,0x002E,0x60,0x00,0x0000,0x0000,0x0000,0x0000,6851,3887,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2454,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,998,SUCCESS
11,2023-08-30 17:05:13,44.079,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0440,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x04,0x0000,0x0000,0x0000,0x0000,6855,700,3890,0,0,26.2,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2458,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1003,SUCCESS
12,2023-08-30 17:05:17,48.083,0x0054,0,65535,26.4,3890,3,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x04,0x0000,0x0000,0x0000,0x0000,6859,700,3890,0,0,26.2,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2462,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1016,SUCCESS
13,2023-08-30 17:05:21,52.091,0x0054,0,65535,26.4,3890,-3,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6863,546,3890,-3,-1,26.2,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2466,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1023,SUCCESS
14,2023-08-30 17:05:25,56.100,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6867,21,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2470,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1014,SUCCESS
15,2023-08-30 17:05:29,60.106,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6871,1,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,-9,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2474,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1038,SUCCESS
16,2023-08-30 17:05:33,64.109,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0440,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6875,0,3890,0,0,26.2,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2478,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1051,SUCCESS
17,2023-08-30 17:05:37,68.110,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6879,0,3890,0,0,26.2,26.4,-273.2,26.4,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2482,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1020,SUCCESS
18,2023-08-30 17:05:41,72.119,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6883,0,3890,0,0,26.2,26.4,-273.2,26.4,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2486,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1042,SUCCESS
19,2023-08-30 17:05:45,76.123,0x0054,0,65535,26.4,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6887,0,3890,0,0,26.1,26.4,-273.2,26.4,-273.2,3890,3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.4,1000,0,0,5,0,2490,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1069,SUCCESS
20,2023-08-30 17:05:49,80.130,0x0054,0,65535,26.6,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6891,575,3890,0,0,26.2,26.6,-273.2,26.6,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.6,1000,0,0,5,0,2494,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1014,SUCCESS
21,2023-08-30 17:05:53,84.136,0x0054,0,65535,26.6,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0440,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6895,3723,3889,0,0,26.3,26.7,-273.2,26.7,-273.2,3889,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.6,1000,0,0,5,0,2498,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1010,SUCCESS
22,2023-08-30 17:05:57,88.142,0x0054,0,65535,26.7,3889,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6899,3723,3889,0,0,26.3,26.7,-273.2,26.7,-273.2,3889,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.7,1000,0,0,5,0,2502,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1019,SUCCESS
23,2023-08-30 17:06:01,92.145,0x0054,0,65535,26.6,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6903,670,3890,0,0,26.3,26.6,-273.2,26.6,-273.2,3890,-6,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.6,1000,0,0,5,0,2506,5103,-28,-11,11,0,2614,5103,-28,11,2.0,1000,4832,2426,882,1031,SUCCESS
24,2023-08-30 17:06:06,96.158,0x0054,0,65535,26.6,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6907,26,3890,0,0,26.3,26.6,-273.2,26.6,-273.2,3890,-3,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.6,1000,0,0,5,0,2510,5103,-28,-11,12,0,2614,5103,-28,12,2.0,1000,4832,2426,882,1020,SUCCESS
25,2023-08-30 17:06:10,100.171,0x0054,0,65535,26.6,3890,0,0,0,69,1730,2513,65535,65535,-3000,35,4500,4400,2500,2600,60,55,0,5,1,150,175,0x10,0,0,0,2500,0x00C0,0,97,0xE180,0x0040,0x10,0x0004,0x40,0x2819,0x0038,0x00,0x00,0x0000,0x0000,0x0000,0x0000,6911,1,3890,0,0,26.3,26.6,-273.2,26.6,-273.2,3890,0,1730,605,2513,919,1728,605,814,325,2514,919,26.3,26.6,1000,0,0,5,0,2514,5103,-28,-11,12,0,2614,5103,-28,12,2.0,1000,4832,2426,882,1021,SUCCESS
Waiting for your reply.
Thanks
Star