To my understanding, a gate driver is a type of power amplifier that accepts a low-power input from a controller IC and produces a high-current drive input for the gate of a high-power MOSFET as shown in the diagram below.

Take the UCC2753x, for example, it says in the datasheet that this driver can drive motors, solenoids etc.
My question is, can I supply the UCC2753x with an AC signal to amplify its current do drive an inductive load directly, as shown in the diagram below?

- If its possible, what are the design steps.
- If its not possible, how do you suggest I drive a 1A current through a coil of inductance 10mH at frequency ranges of (15kHz to 35kHz).
Kind Regards,,,