Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150: No delay and no VGH output?

Part Number: TPS65150

We are finally back working on this circuit from a while back - 

The delays are not working - the outputs are coming on at same time? VO1>VO2 should be ~40ms... it is not.

Also - VO3 is not coming out of the VGH pin. We have 15V on CPI (before shutdown)

CTRL is HIGH, VI is 2.5V

DRVP goes to 15V

Below is scope capture of the power on, showing the voltages starting up and then shutting off;

CH1 (Yellow) is CPI

CH2 (Blue) is VGL

CH3 (Red) is VGH

CH4 ( Green) is AVDD

Please review my schematic and confirm the design.