Other Parts Discussed in Thread: BQ24295,
hi after looking through the BQ256xx and BQ24295 devices I feel like BQ25611D fits my application nicely. I have a few operational questions that I couldn't be 100% sure about from the d/s.
- OTG 5v output is from which pin, PMID or VBUS
- when using battery only, and VBAT > VBAT_DPL and OTG is disabled is there a leakage voltage present at the OTG output pin
- is the SYS 3.5v maintained on both power adaptor and battery or does SYS track VBAT when no adaptor is present
- is there a minimum current draw required on the OTG output for stability
Thanks in advance!
David